SBOSA80 December 2021 REF20-Q1
PRODUCTION DATA
Two types of errors will be discussed: initial accuracy and drift. Accuracy errors include:
It should be noted that these error sources can be greatly reduced at 25ºC by performing a two point system calibration. Drift errors, on the other hand, can only be reduced by performing the calibration over temperature. The drift errors include:
Equation 8 can be used to convert specifications given in parts per million (ppm) to a percentage (%), and vice versa.
Equation 9 can be used to convert specifications given in decibels (dB) to a linear representation.
For some error calculations a full-scale range (FSR) is required. The FSR for this design is determined by the voltage across the shunt resistor, which is ±25 mV (or 50 mV).
For drift errors, the largest change in temperature (ΔT) is 100ºC, which is the difference between the maximum specified temperature (125ºC) and room temperature (25ºC). This temperature change is used when calculating drift errors for the shunt resistor and INA240-Q1. Because the REF20-Q1 uses the box method to determine drift, the temperature range used for calculations is the entire operating range, or 150ºC.
Finally, errors due to CMRR and PSRR specifications require an adjustment depending on the difference between the system’s requirements and how the devices were characterized. For example, the INA240-Q1 was characterized using a common-mode voltage of 12 V. The common-mode voltage in this design is ~0V. This discrepancy causes an input-referred offset voltage.
Below, Table 10-1 summarizes the initial accuracy calculations.
ERROR SOURCE | DEVICE: RSHUNT (PPM) | DEVICE: IN240-Q1 (PPM) | DEVICE: REF2030-Q1 (PPM) | TOTAL (PPM, RSS) |
---|---|---|---|---|
OFFSET | 100 FSR | 500 FSR | 510 FSR | |
CMRR | 60 FSR | 60 FSR | ||
PSRR | 40 FSR | 40 FSR | ||
GAIN ERROR | 1000 | 500 | 1118 | |
TOTAL (PPM, RSS) | 1000 | 1087.5 FSR | 500 FSR | 1231 FSR (0.123%) |
Below, Table 10-2 summarizes the total temperature drift calculations.
ERROR SOURCE | DEVICE: RSHUNT (PPM) | DEVICE: IN240-Q1 (PPM) | DEVICE: REF2030-Q1 (PPM) | TOTAL (PPM, RSS) |
---|---|---|---|---|
OFFSET DRIFT | 100 FSR | 495 | 505 FSR | |
GAIN ERROR DRIFT | 1500 | 50 | 1501 | |
TOTAL (PPM, RSS) | 1500 | 111.8 FSR | 495 | 1583.52 FSR (0.194%) |