SLPS785 December 2023 RES11A
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The resistors of the RES11A are described by the following equations:
RINnom and RGnom are the nominal values of each resistor. The parameter tabs is an error term that describes the absolute tolerance of the RES11A device in question, such that |tabs| ≤ 12%. The absolute tolerance is dominated by the variation in the SiCr resistivity, tSiCr. The four resistors of a given RES11A are interdigitated and come from the same area of the wafer; therefore, tSiCr is effectively the same for each of the four resistors, although tSiCr varies on a part-to-part basis. The following examples show that when each divider is considered in ratiometric terms, these error terms drop out. Parameter tRx is an error term that describes the remaining effective tolerance of each resistor of the given RES11A device after accounting for the universal tSiCr.
The RES11A is specified with a maximum divider ratio tolerance of 0.05%, meaning that the relationship between the actual divider ratio Gx and nominal ratio Gnom of a given divider x is described by the following:
such that tDx ≤ 0.05%. Because any devices that do not meet these criteria are screened out at final test, these equations can be used with Equation 5 to prove the effective bounds of tRx. Therefore, despite the device absolute end-to-end tolerance bounds of ±12%, the effective error tolerances of each resistor (for ratiometric applications) are within approximately ±0.025%, for the worst-case tRx.
The RES11A is specified with a maximum divider matching tolerance of 0.1%, meaning that the relationship between the ratio of divider 1 (G1) and ratio of divider 2 (G2) is described by the following:
By definition, |tM| ≤ 0.1%. Again, the previous equations relate tM to the parameters tDX and tRX. As a result of the interdigitation of the two dividers, the actual typical magnitude of tM is significantly lower than this maximum value, depending on the specific RES11A device. This value is used to calculate the common-mode rejection ratio (CMRR) when implementing a difference amplifier circuit. For example, typical tM for the RES11A40 is approximately 85 ppm, and the typical CMRR is 95.4 dB.