SLLSEM1B February 2015 – April 2015 SN65LVDS93A-Q1
PRODUCTION DATA.
There is no fundamental information about how many layers should be used and how the board stackup should look. Again, the easiest way the get good results is to use the design from the EVMs of Texas Instruments. The magazine Elektronik Praxis has published an article with an analysis of different board stackups. These are listed in Table 3. Generally, the use of microstrip traces needs at least two layers, whereas one of them must be a GND plane. Better is the use of a four-layer PCB, with a GND and a VCC plane and two signal layers. If the circuit is complex and signals must be routed as stripline, because of propagation delay and/or characteristic impedance, a six-layer stackup should be used.
MODEL 1 | MODEL 2 | MODEL 3 | MODEL 4 | |
---|---|---|---|---|
Layer 1 | SIG | SIG | SIG | GND |
Layer 2 | SIG | GND | GND | SIG |
Layer 3 | VCC | VCC | SIG | VCC |
Layer 4 | GND | SIG | VCC | SIG |
Decoupling | Good | Good | Bad | Bad |
EMC | Bad | Bad | Bad | Bad |
Signal Integrity | Bad | Bad | Good | Bad |
Self Disturbance | Satisfaction | Satisfaction | Satisfaction | High |
A complete ground plane in high-speed design is essential. Additionally, a complete power plane is recommended as well. In a complex system, several regulated voltages can be present. The best solution is for every voltage to have its own layer and its own ground plane. But this would result in a huge number of layers just for ground and supply voltages. What are the alternatives? Split the ground planes and the power planes? In a mixed-signal design, e.g., using data converters, the manufacturer often recommends splitting the analog ground and the digital ground to avoid noise coupling between the digital part and the sensitive analog part. Take care when using split ground planes because:
For Figure 22, do not route a signal referenced to digital ground over analog ground and vice versa. The return current cannot take the direct way along the signal trace and so a loop area occurs. Furthermore, the signal induces noise, due to crosstalk (dotted red line) into the analog ground plane.
A right angle in a trace can cause more radiation. The capacitance increases in the region of the corner, and the characteristic impedance changes. This impedance change causes reflections.