SLLS992B August 2009 – March 2015 SN65LVDS93A
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
This section describes the power up sequence, provides information on device connectivity to various GPU and LCD display panels, and offers a PCB routing example.
The SN65LVDS93A does not require a specific power-up sequence.
The device is permitted to power up IOVCC while VCC, VCCPLL, and VCCLVDS remain powered down and connected to GND. The input level of the SHTDN during this time does not matter as only the input stage is powered up while all other device blocks are still powered down.
The device is also permitted to power up all 3.3-V power domains while IOVCC is still powered down to GND. The device will not suffer damage. However, in this case, all the I/Os are detected as logic HIGH, regardless of their true input voltage level. Hence, connecting SHTDN to GND will still be interpreted as a logic HIGH; the LVDS output stage will turn on. The power consumption in this condition is significantly higher than standby mode, but still lower than normal mode.
The user experience can be impacted by the way a system powers up and powers down an LCD screen. The following sequence is recommended:
Power-up sequence (SN65LVDS93A SHTDN input initially low):
Power-down sequence (SN65LVDS93A SHTDN input initially high):
For this design example, use the parameters listed in Table 3 as the input parameters.
DESIGN PARAMETER | EXAMPLE VALUE |
---|---|
VCC | 3.3 V |
VCCIO | 1.8 V |
CLKIN | Falling edge |
SHTDN# | High |
Format | 18-bit GPU to 24-bit LCD |
While there is no formal industry standardized specification for the input interface of LVDS LCD panels, the industry has aligned over the years on a certain data format (bit order). Figure 15 through Figure 18 show how each signal should be connected from the graphic source through the SN65LVDS93A input, output and LVDS LCD panel input. Detailed notes are provided with each figure.
Figure 19 shows a possible breakout of the data input and output signals on two layers of a printed-circuit-board.