The power supply can be any voltage between the minimum and maximum supply
voltage rating located in the Recommended Operating Conditions. Each
VCC terminal should have a good bypass capacitor to prevent power
disturbance. A 0.1-μF capacitor is recommended for this device. It is acceptable to
parallel multiple bypass capacitors to reject different frequencies of noise. The
0.1-μF and 1-μF capacitors are commonly used in parallel. The bypass capacitor
should be installed as close to the power terminal as possible for best results, as
shown in the following layout example.