B. Waveform 1
is for an output with internal conditions such that the output is low except
when disabled by the output control. Waveform 2 is for an output with internal
conditions such that the output is high except when disabled by the output
control.
C. All input
pulses are supplied by generators having the following characteristics: PRR ≤ 1
MHz, ZO = 50 Ω, tr ≤ 3 ns, tf ≤ 3 ns.
D. The outputs
are measured one at a time with one input transition per measurement.