The SN74AHC74Q-Q1 is a clocked device. As such, it
requires special timing considerations for normal operation.
Primary timing factors to consider:
- Maximum clock frequency: the maximum operating
clock frequency defined in Timing Requirements - 74 is the maximum
frequency at which the device is designed to function. This value refers
specifically to the triggering waveform, measuring from one trigger level to the
next.
- Pulse duration: ensure that the triggering event
duration is larger than the minimum pulse duration, as defined in the Timing
Requirements - 74.
- Setup time: ensure that the data has changed at
least one setup time prior to the triggering event, as defined in the Timing
Requirements - 74.
- Hold time: ensure that the data remains in the
desired state at least one hold time after the triggering event, as defined in
the Timing Requirements - 74.