Phase relationships between waveforms
were chosen arbitrarily for the examples listed in the following table. All input
pulses are supplied by generators having the following characteristics: PRR ≤ 1MHz,
ZO = 50Ω, tt < 2.5ns.
For
clock inputs, fmax is measured when the input duty cycle is 50%.
The outputs are measured individually
with one input transition per measurement.
(1) CL includes probe
and test-fixture capacitance.
Figure 6-1 Load Circuit for Push-Pull
OutputsFigure 6-3 Voltage Waveforms, Setup
and Hold Times (1) The greater between
tr and tf is the same as tt.
Figure 6-5 Voltage Waveforms, Input
and Output Transition TimesFigure 6-2 Voltage Waveforms, Pulse
Duration (1) The
greater between tPLH and tPHL is the same as
tpd.
Figure 6-4 Voltage Waveforms
Propagation DelaysNoise values measured with all
other outputs simultaneously switching.
Figure 6-6 Voltage Waveforms, Noise