B. Waveform 1 is for an output with
internal conditions such that the output is low, except when disabled by the
output control. Waveform 2 is for an output with internal conditions such that
the output is high, except when disabled by the output control.
C. All input pulses are supplied by
generators having the following characteristics: PRR ≤ 1 MHz, ZO = 50
Ω, tr ≤ 3 ns, tf ≤ 3 ns.
D. The outputs are measured one at a
time, with one input transition per measurement.
E. tPLZ and
tPHZ are the same as tdis.
F. tPZL and tPZH are the
same as ten.
G. tPHL and
tPLH are the same as tpd.
H. All parameters and waveforms are
not applicable to all devices.