Following common printed-circuit board layout
guidelines are recommended to ensure reliability of the device, which follows:
- Use bypass capacitors on the
power supply pins and place them as close to the device as possible. A 0.1
µF capacitor is recommended, but transient performance can be improved by
having both 1 µF and 0.1 µF capacitors in parallel as bypass
capacitors.
- The high drive capability of
this device creates fast edges into light loads; so routing and load
conditions should be considered to prevent ringing.