As with any high-speed design, there
are many factors which influence the overall performance. The following list
indicates critical areas for consideration during design.
- Use 85 Ω impedance traces
when interfacing with PCIe CEM connectors. Length matching on the P and N
traces should be done on the single-ended segments of the differential
pair.
- Use a uniform trace width and
trace spacing for differential pairs.
- Place AC-coupling capacitors
near to the receiver end of each channel segment to minimize
reflections.
- AC-coupling capacitors of 220 nF are recommended, set the
maximum body size to 0402, and add a cutout void on the GND plane below the
landing pad of the capacitor to reduce parasitic capacitance to GND.
- Back-drill connector vias and
signal vias to minimize stub length.
- Use reference plane vias to
ensure a low inductance path for the return current.