SLOSE86B july 2022 – july 2023 TAS2781
PRODUCTION DATA
This tone generator produces a simple audio tone (beep) that is transmitted directly to the output (speaker).
The generator relies on a pulsed signal coming into either SDZ or NC_SCLK pin.
The beep generation is executed by pulsating any of these two pins with an input frequency fIN specified in .
The beep output signal will have a frequency given by:
For example, if an 800 Hz beep is needed, input a 3.2 kHz PWM signal to pin NC_SCLK.
The beep generation can happen when the device is in Software Shutdown mode, by applying pulses on the pin. A deglitch timer will hold-off the shut-down functionality until the tone has finished and the deglitch timer has expired in which case the pin will revert to controlling the hardware shutdown of the device (SDZ) or SPI clock (NC_SCLK).
The output power of the beep signal is controled by the duty cycle of the input signal as discribed in the table below.
Load (Ω ) | Duty Cycle (% ) | Ouput Power ( W ) |
---|---|---|
8 | 20 - 30 | 0.125 |
8 | 45 - 55 | 0.25 |
8 | 70 - 80 | 0.5 |
Note: When NC_SCLK pin is used for beeping, pin 17 should be connected to an 1.8 V supply (AVDD, IOVDD).