SLASE77A March 2016 – March 2016 TAS5733L
PRODUCTION DATA.
PIN | TYPE(2) | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
ADR/FAULT | 19 | DI/DO | Dual function terminal which sets the LSB of the I²C Address to 0 if pulled to GND, 1 if pulled to AVDD. Also, if configured to be a fault output by the methods described in the Fault Indication section, this terminal will be pulled low when an internal fault occurs. |
AGND | 35 | P | Ground reference for analog circuitry (NOTE: This terminal should be connected to the system ground) |
AMP_OUT_A | 6 | AO | Speaker amplifier outputs |
AMP_OUT_B | 2 | ||
3 | |||
AMP_OUT_C | 46 | ||
47 | |||
AMP_OUT_D | 43 | ||
AVDD | 18 | P | Power supply for internal analog circuitry |
AVDD_REF | 17 | P | Internal power supply (NOTE: This terminal is provided as a connection point for filtering capacitors for this supply and must not be used to power any external circuitry) |
AVDD_REG | 38 | P | Voltage regulator derived from AVDD supply (NOTE: This terminal is provided as a connection point for filtering capacitors for this supply and must not be used to power any external circuitry) |
BSTRP_A | 9 | P | Connection points to for the bootstrap capacitors, which are used to create a power supply for the gate drive for the high-side device |
BSTRP_B | 1 | ||
BSTRP_C | 48 | ||
BSTRP_D | 40 | ||
DGND | 34 | P | Ground reference for digital circuitry (NOTE: This terminal should be connected to the system ground) |
DVDD | 33 | P | Power supply for the internal digital circuitry |
DVDD_REG | 23 | P | Voltage regulator derived from DVDD supply (NOTE: This terminal is provided as a connection point for filtering capacitors for this supply and must not be used to power any external circuitry) |
GVDD_REG | 39 | P | Voltage regulator derived from PVDD supply (NOTE: This terminal is provided as a connection point for filtering capacitors for this supply and must not be used to power any external circuitry) |
LRCLK | 25 | DI | Word select clock for the digital signal that is active on the input data line of the serial port |
MCLK | 20 | DI | Master clock used for internal clock tree and sub-circuit/state machine clocking |
NC(1) | 12 | P | Not connected inside the device (all "no connect" terminals should be connected to system ground) |
13 | |||
30 | |||
36 | |||
37 | |||
OSC_GND | 22 | P | Ground reference for oscillator circuitry (NOTE: These terminals should be connected to the system ground) |
OSC_RES | 21 | AO | Connection point for precision resistor used by internal oscillator circuit. Details for this resistor are shown in the Typical Applications section |
PBTL | 11 | DI | Places the power stage in BTL mode when pulled low, or in PBTL mode when pulled high |
PDN | 24 | DI | Places the device in power down when pulled low |
PGND | 4 | — | Ground reference for power device circuitry (NOTE: This terminal should be connected to the system ground) |
5 | |||
44 | |||
45 | |||
PLL_FLTM | 15 | AO | Negative connection point for the PLL loop filter components |
PLL_FLTP | 16 | AO | Positive connection point for the PLL loop filter components |
PLL_GND | 14 | P | Ground reference for PLL circuitry (NOTE: This terminal should be connected to the system ground) |
PVDD | 7 | P | Power supply for internal power circuitry |
8 | |||
41 | |||
42 | |||
RST | 31 | DI | Places the devices in reset when pulled low |
SCL | 29 | DI | I²C serial control port clock |
SCLK | 26 | DI | Bit clock for the digital signal that is active on the input data line of the serial data port |
SDA | 28 | DI/DO | I²C serial control port data |
SDIN | 27 | DI | Data line to the serial data port |
SSTIMER | 10 | AO | Connection point for the capacitor that is used by the ramp timing circuit, as described in the SSTIMER Pin Functionality section |
TEST | 32 | — | Used by TI for testing during device production (NOTE: This terminal should be connected to system ground) |
PowerPAD | — | P | Exposed metal pad on the underside of the device, which serves as an electrical connection point for ground as well as a heat conduction path from the device into the board (NOTE: This terminal should be connected to ground through a land pattern defined in the Mechanical Data section) |