SLASEH5D May 2018 – November 2020 TAS5805M
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
A combination of digital gain and analog gain is used to provide the overall gain of the speaker amplifier. As seen in Figure 7-7, the audio path of the TAS5805M consists of a digital audio input port, a digital audio path, a digital to PWM converter (DPC), a gate driver stage, a Class-D power stage, and a feedback loop which feeds the output information back into the DPC block to correct for distortion sensed on the output pins. The total amplifier gain consists of digital gain shown in the digital audio path, and the analog gain from the input of the analog modulator to the output of the speaker amplifier power stage.
As shown in Figure 7-7, the first gain stage of the speaker amplifier is present in the digital audio path. Digital gain consists of the volume control, input Mixer or output Crossbar. The digital gain is set to 0dB by default. Change analog gain via register 0x54, AGAIN[4:0] which supports 32 steps analog gain setting (0.5dB per step). These analog gain settings ensure that the output signal is not clipped at different PVDD levels. 0dBFS output corresponds to 29.5-V peak output voltage.
AGAIN <4:0> | GAIN (dBFS) | AMPLIFIER PEAK OUTPUT VOLTAGE (V) |
---|---|---|
00000 | 0 | 29.5 |
00001 | -0.5 | 27.85 |
……. | …….. | ……. |
11111 | -15.5 | 4.95 |