SLOSE88 December 2024 TAS6754-Q1
ADVANCE INFORMATION
TAS6754-Q1 can measure the output current of each channel simultaneously. This functionality is completely integrated and requires no external components.
The channel output current measurement is performed at the rate of the sampling frequency Fs. The measured current amplitude is provided through SDOUT. For more details on the data transmission configuration see SDOUT. Note that the current measurement and the data transmission are two separate functions and both require proper setup before the data can be made available.