SLOSE88 December 2024 TAS6754-Q1
ADVANCE INFORMATION
The TAS6754-Q1 has built-in protections on the charge pump pins (CP, CPC_TOP, and CPC_BOT). When the device detects a fault condition on the charge pins the charge pump will skip a clock cycle. This is considered one fault cycle. The device will then try again on the next incoming clock cycle. If a fault condition is detected two times consecutively or three times in total, the charge pump will start to ignore the incoming clock and go into a Charge Pump Fault condition with the output stage in Hi-Z and charge pump shutdown.
Based on the configuration, a fault signal is generated, which by default generates an active low signal at the FAULT pin.