SCPS204D January 2014 – November 2019 TCA9545A
PRODUCTION DATA.
Following the successful acknowledgment of the slave address, the bus master sends a byte to the TCA9545A, which is stored in the control register (see Figure 15). If multiple bytes are received by the TCA9545A, it saves the last byte received. This register can be written and read via the I2C bus.