SLLSFG2 December 2019 – December 2019 TCAN1044V
PRODUCTION DATA.
The STB pin is an input pin used for mode control of the transceiver. The STB pin can be supplied from either the system processor or from a static system voltage source. If normal mode is the only intended mode of operation than the STB pin can be tied directly to GND.