SLLSFG2 December 2019 – December 2019 TCAN1044V
PRODUCTION DATA.
The TCAN1044V is designed to be an ideal passive or no load to the CAN bus if the device is unpowered. The bus pins were designed to have low leakage currents when the device is unpowered, so they do not load the bus. This is critical if some nodes of the network are unpowered while the rest of the of network remains operational.
The logic pins also have low leakage currents when the device is unpowered, so they do not load other circuits which may remain powered.