SLLSF31A May 2021 – December 2021 TCAN1162-Q1
PRODUCTION DATA
Fail-safe mode is a low power mode in which the TCAN1162-Q1 is in a protected state. While in fail-safe mode the internal regulator (VFLT) is off, the INH pin is off, and the CAN transmitter and receiver are off.
Fail-safe mode is entered if:
Fail-safe mode is exited if all of the following criteria are met:
If the fault condition is not cleared within tINACTIVE then the device will transition into it's lowest power mode, sleep mode.