SNAS854 February 2023 TDC1000-Q1
PRODUCTION DATA
The Multiple Echo mode is intended for use in level sensing applications and distance/displacement measurements in which multiple echoes (burst) are received. In this condition, each received echo group will be treated as a single pulse on the STOP pin. Up to 7 STOP pulses can be generated based on the value of the NUM_RX field in the CONFIG_1 register. Multi echo mode can be enabled by setting the RECEIVE_MODE bit to 1 in the CONFIG_4 register. #SNAS6484660 shows a representation of multiple echo STOP pulse generation.
The rising edge of a STOP pulse is generated by a zero-crossing event. As in the Single Echo Receive Mode, the threshold comparator qualifies the next zero-cross after an RX amplitude smaller than the programmed threshold voltage is detected. The STOP pulse will extend until a zero-cross after the RX amplitude is no longer smaller than the threshold voltage (see #SNAS6488072).
If the number of expected pulses programmed in NUM_RX is not received or the time-of-flight operation times out, the TDC1000-Q1 will indicate an error condition in the ERROR_FLAGS register and will set the ERRB pin low.