SNLS698A April 2021 – September 2023 TDES960
PRODUCTION DATA
A frame synchronization signal (FrameSync) can be sent through the back channel using any of the back channel GPIOs. The signal can be generated in two different methods. The first option offers sending the external FrameSync using one of the available GPIO pins on the TDES960 and mapping that GPIO to a back channel GPIO on one or more of the V3Link ports.
The second option is to have the TDES960 internally generate a FrameSync signal to send through GPIO to one or more of the attached Serializers.
FrameSync signaling on the four back channels is synchronous. Thus, the FrameSync signal arrives at each of the four serializers with limited skew.