SBOS780C March 2016 – June 2021 THS3215
PRODUCTION DATA
The distortion plots for all stages used a filtered high-frequency function generator to generate a very low-distortion input signal. The LMH3401 interface was used when testing the D2S and the full-signal path (D2S + OPS) harmonic distortion performance. Running the filtered signal through the LMH3401, as shown in Figure 7-4, provided adequate input signal purity because of the approximately –100-dBc harmonic distortion performance through 100 MHz provided by the LMH3401. In order to test the harmonic-distortion performance of the OPS and midscale buffer, the configuration shown in Figure 7-5 was used.