Achieving optimum performance with a high-frequency amplifier such as the THS3491 requires careful attention to board layout parasitic and external component types.
Recommendations that optimize performance include:
- Minimize parasitic capacitance to any AC ground for all of the signal I/O pins. Parasitic capacitance on the output and input pins can cause instability. To reduce unwanted capacitance, a window around the signal I/O pins must be opened in all of the ground and power planes around those pins. Otherwise, ground and power planes must be unbroken elsewhere on the board.
- Minimize the distance (< 0.25 of an inch [6.35 mm] from the power supply pins to high-frequency 0.1-μF and 100-pF decoupling capacitors. At the device pins, the ground and power plane layout must not be in close proximity to the signal I/O pins. Avoid narrow power and ground traces to minimize inductance between the pins and the decoupling capacitors. The power supply connections must always be decoupled with these capacitors Use larger tantalum decoupling capacitors (with a value of 6.8 µF or more) that are effective at lower frequencies on the main supply pins. These can be placed further from the device and can be shared among several devices in the same area of the printed circuit board (PCB).
- Careful selection and placement of external components preserve the high-frequency performance of the THS3491. Resistors must be a low reactance type. Surface-mount resistors work best and allow a tighter overall layout. Keep leads and PCB trace length as short as possible. Never use wire-bound type resistors in a high-frequency application. Because the output pin and inverting input pins are the most sensitive to parasitic capacitance, always position the feedback and series output resistors, if any, as close to the inverting input pins and output pins as possible, respectively. Place other network components such as input termination resistors close to the gain setting resistors. Even with a low parasitic capacitance shunting the external resistors, excessively high resistor values create significant time constants constraints? that can degrade performance. Good axial metal film or surface-mount resistors feature approximately 0.2 pF capacitance in shunt with the resistor. For resistor values greater than 2 kΩ, this parasitic capacitance adds a pole or a zero that can effect circuit operation. Keep resistor values as low as possible and consistent with load-driving considerations.
- Make connections to other wideband devices on the board with short direct traces or through onboard transmission lines. For short connections, consider the trace and the input to the next device as a lumped capacitive load. Use relatively wide traces of 0.05 inch to 0.1 inch (1.3 mm to 2.54 mm), preferably with open ground and power planes around the traces. Estimate the total capacitive load and determine if isolation resistors on the outputs are required. Low parasitic capacitive loads ( less than 4 pF) may not require series resistance because the THS3491 is nominally compensated to operate with a 2-pF parasitic load. Higher parasitic capacitive loads without a series resistance are allowed as the signal gain increases (increasing the unloaded phase margin). If a long trace is required and the 6-dB signal loss intrinsic to a twice-terminated transmission line is acceptable, implement a matched impedance transmission line using microstrip or stripline techniques (consult an ECL design handbook for microstrip and stripline layout techniques).
- A 50-Ω environment is not required onboard, and a higher impedance environment
improves distortion as shown in the distortion
versus load plots; see GUID-E5F9035E-1746-4A47-8531-1DFCA205BA30.html#X112 and GUID-E5F9035E-1746-4A47-8531-1DFCA205BA30.html#SBOS875_THS3491878. With a characteristic board trace impedance
based on board material and trace dimensions, a
matching series resistor into the trace from the
output of the THS3491 is used. A
terminating shunt resistor at the input of the
destination device is also used. The terminating
impedance is the parallel combination of the shunt
resistor and the input impedance of the
destination device. This total effective impedance
must be set to match the trace impedance.
If the 6-dB attenuation
of a twice-terminated transmission line is
unacceptable, a long trace can be series
terminated at the source end only. Treat the trace
as a capacitive load in this case. This
termination does not preserve signal integrity as
well as a twice-terminated line. If the input
impedance of the destination device is low, there
is some signal attenuation because of the voltage
divider formed by the series output into the
terminating impedance. - Do not socket a high-speed device like the THS3491. The socket introduces additional lead lengths and pin-to-pin capacitance, which can create a troublesome parasitic network. This can make it achieving a smooth, stable frequency response impossible. Obtain better results by soldering the THS3491 devices directly onto the board.