SBOS831B December 2016 – June 2021 THS4552
PRODUCTION DATA
Probing the response to the output pins by using the THS4552 SBOC471 TINA-TI™ simulation model (before the RC filter to the SAR ADC) illustrates the expected response plus some peaking at higher frequencies. Any signal or noise peaking that appears at the output because of this peaking is rolled off by the RC filter between the FDA and SAR inputs. A place for a differential input capacitor is illustrated in Figure 9-14 (as 0.1 pF) but is not used for this simulation. This slight peaking is a combination of low phase margin and feedthrough via the feedback capacitor to the increasing open-loop output impedance of Figure 8-3. The loop gain and phase response are available as a TINA-TI™ simulation file.
Obtaining the SNR to the ADC input pins, and assuming an 8 VPP full scale (2.83 VRMS), gives the result of Figure 9-16. The 113 dB SNR shown in Figure 9-16 does not limit the performance for any SAR application.