SBOS877A April 2018 – September 2018 THS6301
PRODUCTION DATA.
For maximum performance and reliability, the designer must ensure that the design does not exceed a junction temperature of 125°C. Between 125°C and 150°C, damage does not occur, but the performance of the amplifier begins to degrade and long-term reliability suffers. The thermal characteristics of the device are dictated by the package and the PCB. Equation 1 calculates maximum power dissipation for a given package:
where
For systems where heat dissipation is more critical, the THS6301 is offered in an 16-pin VQFN package with thermal pad. Because of the thermal pad, the thermal coefficient for the VQFN package is substantially improved over the traditional SOIC. The data for the VQFN packages with thermal pad assume a board layout that follows the thermal pad layout guidelines referenced in this section and detailed in the Quad Flatpack No-Lead Logic Packages application note. If the thermal pad is not soldered to the PCB, the thermal impedance increases substantially, which may cause serious heat and performance issues. Be sure to always solder the thermal pad to the PCB for optimum performance.
When determining whether or not the device satisfies the maximum power dissipation requirement, consider not only quiescent power dissipation, but also dynamic power dissipation. Often times, this dissipation is difficult to quantify because the signal pattern is inconsistent, but an estimate of the RMS power dissipation can provide visibility into a possible problem.