SLLSF32C November 2018 – March 2019 THVD1419 , THVD1429
PRODUCTION DATA.
Inductive loads such as relays, switch contactors, or heavy-duty motors can create high-frequency bursts during transition. The IEC 61000-4-4 test is intended to simulate the transients created by such switching of inductive loads on AC power lines. Figure 20 shows the voltage waveforms in to 50-Ω termination as defined by the IEC standard.
Internal ESD protection circuits of the THVD14x9 protect the transceivers against EFT ±4 kV.