SLLSFS6A September 2024 – December 2024 TIOL221
PRODMIX
Refer to the PDF data sheet for device specific package drawings
The TIOL221 has three separate thermal sensors: one for each of the driver and another one for the LDO.
If the die temperature around the CQ driver exceeds T(WRN), the NFLT1 flag is held low indicating a potential over temperature problem. When the TJ exceeds T(SDN), the CQ driver is disabled. The LDO and DO driver remain operational as long as the respective thermal sensors do not exceed T(SDN). As soon as the temperature drops below the temperature threshold (and after T(HYS)), the internal circuit re-enables the driver, subject to the state of the EN1 and TX1 pins.
If the die temperature around the DO driver exceeds T(WRN), the NFLT2 flag is held low indicating a potential over temperature problem. When the TJ exceeds T(SDN), the DO driver is disabled. The LDO and CQ driver remain operational as long as the respective thermal sensors do not exceed T(SDN). As soon as the temperature drops below the temperature threshold (and after T(HYS)), the internal circuit re-enables the driver, subject to the state of the EN2 and TX2 pins.
The thermal sensor near the LDO detects the temperature exceeding the T(SDN). The LDO and both the drivers are turned off and RESET is held low. As soon as the temperature drops below the temperature threshold (and after T(HYS)), the internal circuit re-enables the LDO and the drivers and RESET is released after the VOUT is above the UVLO threshold.