SBAS980B June 2019 – June 2020 TLA2518
PRODUCTION DATA.
In the on-the-fly mode of operation, the analog input channel is selected, as shown in Figure 32, using the first five bits on SDI without waiting for the CS rising edge. Thus, the ADC samples the newly selected channel on the CS edge and there is no latency between the channel selection and the ADC output data.
Figure 32. Starting Conversions and Reading Data in On-the-Fly Mode The number of clocks required for reading the output data depends on the device output data frame size; see the Output Data Format section for more details.