SLIS187C June 2021 – March 2022 TLC6A598
PRODUCTION DATA
Figure 9-5 shows a typical application circuit with TLC6A598 to drive Relays. The MCU generates all the input signals.
Please note that inductive loads, such as stepper motors or relays, can generate negative transients on the DRAINx pins of the device. Typically, this event occurs when the output channel FET turns ON, pulling the DRAINx node to ground. This event can cause the DRAINx node to go below the voltage rating listed in the Absolute Maximum Ratings table, which in effect causes excessive ground current leakage.