SLASEK2A December 2017 – August 2018 TLC6C5724-Q1
PRODUCTION DATA.
As the backlighting includes 128 zones, each TLC6C5724-Q1 device can drive 24 zones, so a total of six TLC6C5724-Q1 units are needed.
According to Maximum Constant-Sink-Current Setting, to realize a 50-mA output current, users can choose a 0.96-kΩ reference resistor.
Users can use a daisy chain connection to control all of the six TLC6C5724-Q1 devices through one serial interface, just as Figure 31 shows. Figure 32 shows how to send the data into cascaded devices, where M is the number of cascading devices.
Figure 32. Cascading Data Write