SLLSFF6 September 2021 TLIN1024A-Q1
PRODUCTION DATA
When using the TLIN1024A-Q1 in systems which are monitoring the RXD pin for a wake-up request, special care should be taken during the mode transitions. The output of the RXD pin is indeterminate for the transition period between states as the receivers are switched. The application software should not look for an edge on the RXD pin indicating a wake-up request until tMODE_CHANGE when going from sleep or standby to normal mode. This is shown in Figure 8-14