SLLSFE4A May 2022 – December 2022 TLIN1431-Q1
PRODUCTION DATA
Sleep Mode is the power saving mode for the TLIN1431x-Q1. Even with extremely low current consumption in this mode, the device can still wake up from the LIN bus through a wake up signal or local wake via WAKE pin. Upon a wake event the SWE timer, tINACT_FS, starts and the device enters restart mode. If UVCC is still present after this time, the device re-enters sleep mode. The LIN bus is filtered to prevent false wake up events. The wake-up events must be active for the respective time periods (tLINBUS).
In pin control mode, sleep mode is entered by setting EN low for longer than tEN and TXD pin is low when entered from normal mode.
In SPI control mode, setting register 8'h1D[7:6] = 01b transitions the device into sleep mode. If the reset counter exceeds three, the device enters sleep mode from restart mode. The reset counter increments on an UVCC event, or a watchdog error event that causes the device to enter restart mode when fail-safe mode is disabled. The reset counter must be cleared through a SPI command.
While the device is in sleep mode, the following conditions exist.
Figure 8-34 Sleep Mode Pin Control | Figure 8-35 Sleep Mode SPI Control |