SLLSFE4A May 2022 – December 2022 TLIN1431-Q1
PRODUCTION DATA
The TLIN1431x-Q1 has multiple functional modes of operation, Init, pin/SPI Init, normal, standby, sleep, restart and fail-safe. The next sections describe these modes as well as how the device moves between the different modes. Figure 8-24 and Figure 8-25 graphically shows the relationship while Table 8-4 and tables show the state of pins in each control mode. Upon power up, and once VCC ≥ UVCC prior to tINACT_FS timing out the device enters an initialization mode (INIT). While in this mode, VCC is ramping, nRST ramps with VCC, all other pins are off except for monitoring the state of the Pin/nCS pin to determine which control method is being implemented. Once the control method is determined, the device follows the pin control or SPI control path of the state diagram.
Function | Restart Mode | Sleep Mode | Standby Mode | Normal Mode | Fail-safe Mode | Fast Mode |
---|---|---|---|---|---|---|
EN | NA | Low | Low | High | NA | Pulse then high |
RXD | High | Floating | Low for a wake event and power up event otherwise high | Mirrors LIN bus | Floating | Mirrors LIN bus |
LIN BUS Termination | Weak current pull-up | Weak current pull-up | 45 kΩ (typical) | 45 kΩ (typical) | Weak current pull-up | 45 kΩ (typical) |
Vbat Voltage Divider | Off | Off | On | On | Fault dependent | On |
Transmitter | Off | Off | Off | On | Off | On (Slope control off) |
Watchdog | Off | Off | On with long first pulse | On | Off | On but only sets flag |
nRST Pin | Low | Low | High | High | LDO state dependent | High |
WAKE Pin | Off | On | On | Off | On | Off |
WKRQ/INH | On | Off | On | On | INH - On; WKRQ - Fault dependent | On |
LIMP |
| Off | Previous state prior to entering STBY due to WD fault | Previous state prior to entering normal mode due to WD fault | On | Previous state prior to entering fast mode due to WD fault |
HSS | Off | Off | On and controlled by HSSC pin | On and controlled by HSSC pin | Off | On and controlled by HSSC pin |
VCC | Ramping | Off | On | On | Fault dependent | On |
Comment | nRST is internally connected to the LDO output which in sleep mode is off | Wake up event detected, waiting on processors to set EN | LIN transmission up to 20 kbps | LDO off for TSD, VCCSC or OVCC events | LIN transmission up to 200 kbps |
LDO state for fault dependent in fail-safe mode is as follows:
If TXD is held dominant when device enters normal or fast modes, the LIN transmitter does not turn on until the TXD pin goes recessive.
If VSUP is ≤ UVSUP WKRQ/INH is off.
WKRQ depends upon the LDO being on, so any event that causes the LDO to be turned off will turn off WKRQ.
Any WD failure in Fast Mode will only set interrupt and not take any other action (will not set LIMP, transition to Fail-safe or Restart or take any WD fail action)
Function | Restart Mode | Sleep Mode | Standby Mode | Normal Mode | Fail-safe Mode | Fast Mode |
---|---|---|---|---|---|---|
RXD | High | Floating | Low for a wake event and power up event otherwise high | Mirrors LIN bus | Fault dependent | Mirrors LIN bus |
LIN BUS Termination | Weak current pull-up | Weak current pull-up | 45 kΩ (typical) | 45 kΩ (typical) | Weak current pull-up | 45 kΩ (typical) |
Vbat Voltage Divider | Off | Off | On | On | Fault dependent | On |
Transmitter | Off | Off | Off | On | Off | On (Slope control off) |
Watchdog | Off | Off | Default on with long first window but programmable off | On If programmed off in standby mode when entering normal mode a long first window is implemented | Off | On but only sets flag |
SPI pins | Off | Off | On | On | Fault dependent | On |
nINT pin | Off | Off | On | On | Fault dependent | On |
nRST pin | Low | Low | High | High | LDO state dependent | High |
WAKE Pin | Off | On | On | Off | On | Off |
WKRQ/INH | On | Off | On | On | INH - On; WKRQ - Fault dependent | On |
LIMP |
| Off | Previous state prior to entering STBY due to WD fault | Previous state prior to entering normal mode due to WD fault | On | Previous state prior to entering fast mode due to WD fault |
HSS | Off | Off unless cyclic sensing enabled | On | On | Off | On |
VCC | Ramping | Off | On | On | Fault dependent | On |
Comment | nRST is internally connected to the LDO output which in sleep mode is off | Wake up event detected, waiting on processors | LIN transmission up to 20 kbps | LDO off for TSD, VCCSC or OVCC events | LIN transmission up to 200 kbps |
Function status when in fail-safe mode that states fault dependent are defined in Table 8-6
If TXD is held dominant when device enters normal or fast modes, the LIN transmitter does not turn on until the TXD pin goes recessive.
If VSUP is ≤ UVSUP WKRQ/INH is off.
WKRQ depends upon the LDO being on, so any event that causes the LDO to be turned off will turn off WKRQ.
Any WD failure in Fast Mode will only set interrupt and not take any other action (will not set LIMP, transition to Fail-safe or Restart or take any WD fail action)
Function | Watchdog Error | Thermal Shutdown | UVCC | VCC Over Voltage | VCCSC | Restart Counter Exceeded |
---|---|---|---|---|---|---|
LDO (2) | On | Off | On | Off | Off | On (1) |
INH | Programmed | On | On | On | On | On |
WKRQ | Programmed | Off | Off | Off | Off | On |
SPI | On | Off | On | Off | Off | On |
Normal mode can be entered from Fast mode with TXD in either state: