SNOSDJ3 May 2024 TLV1812-EP
ADVANCE INFORMATION
The basic comparator configuration may oscillate or produce a noisy "chatter" output if the applied differential input voltage is near the comparator's offset voltage. This usually occurs when the input signal is moving very slowly across the switching threshold of the comparator.
This problem can be prevented by the addition of hysteresis or positive feedback.
The hysteresis transfer curve is shown in Figure 6-2. This curve is a function of three components: VTH, VOS, and VHYST:
For more information, see the Comparator with and without hysteresis circuit application note.