SNOSDG0 August 2024 TLV1H103-SEP
PRODUCTION DATA
The TLV1H103-SEP can be used in conjunction with a high performance amplifier such as the OPA858 to create an optical receiver as shown in the figure below. The photodiode is connected to a bias voltage and is being driven with a pulsed laser. The OPA858 takes the current conducting through the diode and translates the current into a voltage for a high speed comparator to detect. The TLV1H103-SEP then outputs the proper output level according to the threshold set (VREF).