All decoupling capacitors should be located as close as possible to the loads they are supplying.
Large copper fill areas or thick traces are recommended wherever possible to provide low inductance current paths between decoupling capacitors and their loads
Ensure that there are no vias or discontinuities in the forward or return current paths that can cause the current loop area and therefore the loop inductance to increase.
For high-frequency current paths routed across PCB layers, multiple vias can be placed close together (but not obstructing the current path) to lower inductance.