SBOSAG5 December 2024 – December 2024 TLV2888
PRODMIX
Refer to the PDF data sheet for device specific package drawings
A common systems requirement is to monitor the current being delivered to a load. Monitoring confirms that normal current levels are being maintained, and also provides an alert if an overcurrent condition occurs.
Fortunately, a relatively simple current monitor circuit can be achieved using a precision op amp, such as the TLVx888. This device has exceptional precision and wide gain bandwidth product to accommodate for very high gain configurations.
The TLVx888 is configured as a difference amplifier with a predetermined gain. The difference amplifier inputs are connected across a sense resistor through which the load current flows. The sense resistor can be connected to the high side or low side of the circuit through which the load current flows. Commonly, high-side current sensing is applied. Figure 7-3 shows an applicable TLVx888 configuration. Low-side current sensing can be applied as well if the sense resistor can be placed between the load and ground.
Use the following parameters for this design example:
The following design details and equations can be used to reconfigure this design for different output voltage ranges and current loads.