SBOSAG5 December 2024 – December 2024 TLV2888
PRODMIX
Refer to the PDF data sheet for device specific package drawings
The TLVx888 features a proprietary input stage design that allows an input differential voltage to be applied while maintaining high input impedance. Typically, high-voltage CMOS or bipolar-junction input amplifiers feature antiparallel diodes that protect input transistors from large VGS voltages that can exceed the semiconductor process maximum and permanently damage the device. Large VGS voltages can be forced when applying a large input step, switching between channels, or attempting to use the amplifier as a comparator.
The TLVx888 solves these problems with a switched-input technique that prevents large input bias currents when large differential voltages are applied. This input architecture addresses many issues seen in switched or multiplexed applications, where large disruptions to RC filtering networks are caused by fast switching between large potentials.Figure 6-3 shows a typical application where MUX-Friendly inputs can improve settling time performance. The TLVx888 offers outstanding settling performance as a result of these design innovations and built-in slew-rate boost and wide bandwidth. The TLVx888 can also be used as a comparator. Differential and common-mode input ranges still apply.