SBAS906 March 2018 TLV320ADC3100
PRODUCTION DATA.
In I2S mode, the MSB of the left channel is valid on the second rising edge of the bit clock after the falling edge of the word clock. Similarly, the MSB of the right channel is valid on the second rising edge of the bit clock after the rising edge of the word clock. Figure 19 shows the standard I2S timing.
Figure 20 shows the I2S mode timing with Ch_Offset_1 = 2.
Figure 21 shows the I2S mode timing with Ch_Offset_1 = 0 and the bit clock inverted.
For the I2S mode, the number of bit clocks per channel must be greater than or equal to the programmed word length of the data. Also, the programmed offset value must be less than the number of bit clocks per frame by at least the programmed word length of the data.