SLVSHD5 November 2024 TLV61047
PRODUCTION DATA
The device is designed to operate from an input voltage supply range between 2.6V to 20V. This input supply must be well regulated. If the input supply is located more than a few inches from the converter, additional bulk capacitance may be required in addition to the ceramic bypass capacitors. A typical choice is an electrolytic or tantalum capacitor with a value of 47µF. Output current of the input power supply must be rated according to the supply voltage, output voltage and output current of the TLV61047.