SLVSEX0A March 2019 – July 2019 TLV61048
PRODUCTION DATA.
The device is designed to operate from an input voltage supply range between 1.5 V to 5.5 V. This input supply must be well regulated. If the input supply is located more than a few inches from the converter, additional bulk capacitance may be required in addition to the ceramic bypass capacitors. A typical choice is an electrolytic or tantalum capacitor with a value of 47 µF. Output current of the input power supply must be rated according to the supply voltage, output voltage and output current of the TLV61048.