SNVSAV2B January 2018 – November 2019 TLV6700
PRODUCTION DATA.
Some applications monitor rails other than the one that is powering VDD. In these types of applications the resistor divider used to set the desired thresholds is connected to the rail that is being monitored.
NOTE:
The inputs can monitor a voltage higher than VDDmax with the use of an external resistor divider network.