SBOS865B January 2018 – November 2019 TLV6703
PRODUCTION DATA.
Do connect a 0.1-µF decoupling capacitor from VDD to GND for best system performance.
If the monitored rail is noisy, do connect a decoupling capacitor from the comparator input (sense) to GND.
Don't use resistors for the voltage divider that cause the current through them to be less than 100 times the input current of the comparator without also accounting for the effect to the accuracy.
Don't use a pullup resistor that is too small, because the larger current sunk by the output then exceeds the desired low-level output voltage (VOL).