SBVS352A April 2018 – December 2018 TLV759P
PRODUCTION DATA.
The enable pin (EN) is active high. Enable the device by forcing the EN pin to exceed VEN(HI). Turn off the device by forcing the EN pin to drop below VEN(LO). If shutdown capability is not required, connect EN to IN.
The TLV759P has an internal pulldown MOSFET that connects an RPULLDOWN resistor to ground when the device is disabled. The discharge time after disabling depends on the output capacitance (COUT) and the load resistance (RL) in parallel with the pulldown resistor (RPULLDOWN). Equation 1 calculates the time constant: