SBVS157E April 2011 – December 2020 TLV803 , TLV853
PRODUCTION DATA
The TLV803 has built-in rejection of fast transients on the VDD pin. The rejection of transients depends on both the duration and the amplitude of the transient. The amplitude of the transient is measured from the bottom of the transient to the negative threshold voltage of the TLV803, as shown in Figure 8-1.
The TLV803 does not respond to transients that are fast duration/low amplitude or long duration/small amplitude. Transients meeting or longer than the tw specified in the switching characteristics section triggers a reset.