SBOSAJ3 June 2024 TLV9104-Q1
PRODMIX
The TLV910x-Q1 family has internal phase-reversal protection. Many op amps exhibit a phase reversal when the input is driven beyond the linear common-mode range. This condition is most often encountered in noninverting circuits when the input is driven beyond the specified common-mode voltage range, causing the output to reverse into the opposite rail. The TLV910x-Q1 is a rail-to-rail input op amp, therefore the common-mode range can extend up to the rails. Input signals beyond the rails do not cause phase reversal. Instead, the output limits into the appropriate rail. Figure 6-2 shows this performance.