SBOSAJ4 June 2024 TLV9304-Q1
PRODMIX
Many different systems require controlled voltages across numerous system nodes to ensure robust operation. A comparator can be used to monitor and control voltages by comparing a reference threshold voltage with an input voltage and providing an output when the input crosses this threshold.
The MUX-friendly input stage of TLV930x-Q1 op amp family allow designers to use these devices as high voltage comparators (see Input Protection Circuitry). Previous generation high-voltage op amps often use back-to-back diodes across the inputs to prevent damage to the op amp, which greatly limited a designer's capability to use these op amps as comparators. The patented input stage of the TLV930x-Q1, however, allows the device to have a wide differential voltage between the inputs.