SLVSGJ7 April 2022 TLVM13640
PRODUCTION DATA
Connect a resistor, designated as RRT in Figure 8-1, between RT and AGND to set the swiching frequency within the range of 200 kHz to 2.2 MHz. Use Equation 5 or refer to Figure 7-8 to calculate RRT for a desired frequency.
Refer to Table 8-1 or use the simplified expression in Equation 6 to find a switching frequency that sets an inductor ripple current of 30% to 50% of the 4-A module current rating at nominal input voltage:
where
Note that a resistor value outside of the recommended range can cause the module to shut down. This prevents unintended operation if the RT pin is shorted to ground or left open.