SLYS053B November 2023 – June 2024 TMAG3001
PRODUCTION DATA
The TMAG3001 is sensitive to both positive and negative magnetic fields. the device can be configured to act as a switch that is sensitive to a single direction on any of the three axes. Figure 7-10 shows an example for unipolar switch mode where the Bop represents the operating point for the switch above which the INT pin switches to ON state. Brp, represents the reverse operating point, below which the INT pin returns to the OFF operating state. TMAG3001 enables the device to be used as a 3D magnetic switch when all the magnetic channels are enabled and when THR_SEL[1:0] bits are set to 2h. When used as a 3D magnetic switch, INT pin switches to ON state, if one of the magnetic channels crosses the operating point, set by the low thresholds that can be configured in THR_Config1, THR_Config2 and THR_Config3. The hysteresis for the switch mode is set using the THR_HYST bits. The switch turns to an off position only if the measurements of all the enabled magnetic channels fall below the reverse operating point, Brp.